DUG_Unica PB Dimmer_WH-04

About the device

The Connected Universal Push Button Dimmer LED (hereinafter referred to as Dimmer) is a push button device that can be used to switch and dim LED, ohmic, inductive or capacitive loads manually or remotely.

Control options

Home control: To control the dimmer through the Wiser app you will need the Wiser Hub.

Direct operation: The dimmer can always be controlled directly on-site. You can also connect any number of mechanical push buttons.

Functions

  • The device can detect the load automatically.

  • It provides thermal protection, overload-resistance and short-circuit protection.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?