About the device
The thermostat consists of:
-
Connected Thermostat Insert 2 A (MEG5777-0000)
-
Frame
-
Connected Thermostat Module, ZB (MEG5779-0xxx)
The thermostat is composed of three components: inserts, frame, and ZB module, and each must be ordered separately.
Thermostat features:
-
Measure & control the room temperature
-
Dot-matrix displays (current room and set temperature)
-
Device lock
-
Valve Protection
-
Heat/cool changeover
-
Universal input setback/presence (external)
-
Volt-free or live control, normally open or normally closed.
-
Smart schedule through a Wiser app
Operating elements
-
Dot-matrix display
TIP: All LED indications are explained in the LED behavior chapter. -
Rotary push-button