DUG_Push-button Module, 1-gang/2-gang_WH-06

Adjusting the brightness level

To increase/decrease the brightness level:

  1. On the Control tab, tap All devices or the room tab where the device is located.

  2. Tap (A) to turn On/Off the light.

  3. Tap Dimmer (B) to set brightness % using the sliding bar.

    TIP:
    • You can also tap to turn On/Off the light.

    • Additionally, you can turn the device On/Off and adjust the brightness from the Home screen when you add it to your Favourite. To know more about Favourite, refer to the Managing Favourites topic in the respective System User Guide.

    • Use Follow schedule switch (C) to turn On and Off the schedule and tap Edit schedule (D) to edit the created schedule.

    Tap Add as favourite (E) to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to the Managing Favourites topic in the respective System User Guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?