DUG_Wiser_Airzone_WH-05

Operating modes

Using the Wiser Home app, you can manage the operating modes for Airzone devices.
  1. On the Control tab, tap All devices or a room tab where the Airzone device is located.
  2. On the device control screen, tap (A).
    The operating modes (B) will be shown according to the connected Airzone device.

  3. Select any one of the available modes (B):
    • Heating

    • Cooling

    • Dry

    • Ventilation

    • Stop

  4. Drag the sliding bar up/down (C) to adjust the set-point temperature (Heating, Cooling and Dry) or tap on the icon of the operating mode to activate/deactivate it.
    TIP: You can also adjust the set-point temperature:
    • By tapping or of the heating, cooling or dry section on the Control tab.

    • When you add it to your Favorites. To know more about Favourite, refer to the Managing Favourites topic in the respective System User Guide.

    NOTE: If you only have a single device in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen.

    Room settings: You can edit the room name for the device.

    The current operating mode indicates the mode in which the system is working.
    • Off : Turns the system off.
    • Heating : System operates in heating mode when the set-point temp > room temp.
    • Cooling : System operates in cooling mode when the set-point temp < room temp.
    • Dry : System operates in dry mode, reducing the humidity and refreshing the environment when set-point temp < room temp.
    • Ventilation :System operates in fan mode when set-point temp < room temp.
    • Stop : When the set-point temperature has reached, the AC unit remains switched on in low consumption mode (Stand-by mode).
    • Boost mode: Boost Mode will apply a boost of +2 °C for one hour to every room in the system. For more information on different modes, refer to Boost Mode.
    • Auto mode :(This mode is available only for Aidoo) Enables automatic switching between cooling and heating and can turn off when required.
      IMPORTANT: Auto mode can be activated only via the Airzone app.
    NOTE: To access live, history and energy insights, it’s recommended to install PowerTag on the Airzone loads. Refer to Checking device consumption.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?