DUG_Unica PB Dimmer_WH-04

Creating a moment

  1. On the Home page, tap .
  2. Go to Moments and then tap to create a moment.
  3. Enter the name of the moment (A).
    TIP: You can choose the cover image that represents your moment by tapping .
  4. Tap Add actions (B) to select the list of devices.
  5. In the Add actions menu, you can select the devices (C).
  6. Once the device are selected, tap Done.
  7. On the Moment creator page, tap the device to set the condition. For example if it is a dimmer:
    • Tap to turn on (D)
    • Drag the sliding bar up/down to increase/decrease the brightness (E) and tap Set on the upper right corner.
  8. After setting all conditions, tap Save.
    Once the moment is saved, it will appear on the Moments tab. Tap on the moment to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?