DUG_Unica Relay Switch_WH-03

Editing an automation

  1. On the Home page, tap .
  2. Go to Automation, tap the automation you want to edit.
  3. On the Edit automation page, you can perform following changes:
    • Change the icon .

    • Rename the automation.

    • Tap each condition to change the settings.

      • To remove a condition, slide the condition towards left and then tap (A) to delete it.

      • Tap ⊕ Add conditions (B) to add new condition.

  4. Tap Save , to save the changes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?