DUG_PowerTag-E_WH-07

Energy view of individual devices

You can monitor more devices in the powerflow in the Energy tab. You can view the energy consumption in kWh on a daily, weekly, monthly and yearly basis.

The powerflow will display instant power of these devices if you have installed them.

  • Smart Plugs

  • Connected Sockets

  • 16 A Relays

Advantages:

  • Live data of individual devices.

  • History of individual devices.

Pre-requisite: Pair smart plugs and connected sockets by assigning an icon. The new icon will be displayed on the home screen and energy breakdown.
If you are pairing the devices with Wiser Hub for the first time, refer to Pairing the Connected socket, Pairing Smart Plug.
If you have already installed the devices and want to change the device icon, refer to Changing the icon for Smart Plugs, Connected sockets.
NOTE: Changing the icon to another category will delete all the historical data.

Once the Wiser Home app is updated, user gets notified that powerflow feature is available for the mentioned devices in the Energy tab.

  1. Read the feature update and swipe to navigate to next screen.

  2. Tap to close the overlay screen.

Live

To access the live data:
  1. On the bottom navigation bar, tap > Live.

    Powerflow and Live graph is shown for 16 A relays , smart plugs and connected sockets only if there is an energy source. (Display up to 4 highest devices).

History

To access energy history:
  1. On the bottom navigation bar, tap > History.

  2. Tap (A) to select a required time frame (A): Hours, Days, Months, Years.

    The history for the installed devices is highlighted in the graph (B).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?