DUG_Smoke alarm DC_WH-03

Example of an automation

In the example below, you will get a notification in your app when smoke is detected.
  1. Go to Automation > to create an automation.
  2. To add a condition, tap Add Condition > Device status change > Smoke Alarm.
  3. In Select function menu tap on Smoke Alarm (A).
  4. To change the status as Smoke Detected, tap > Set.
  5. To add an action, tap Then > Add an action > Send notification > Notify me.
  6. Read the information and tap OK.
  7. Enter the name of the automation and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .
    You can enable or disable saved automations on the Automation tab by using (B).
You will receive notification when the automation is triggered.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?