DUG_PowerTag-E_WH-08

Installing the device

It is recommended to install the PowerTag within 3 metres of the Wiser Hub for best results. This provides a good network strength and helps to prevent online/offline issues, which might result in corrupting data. The signal quality is best maintained when there are no big obstructions (for example thick walls, metal cabinets etc.) between the PowerTag & Wiser Gateway/Hub. Refer to the installation instruction supplied with this product.

Instruction manual links:

Installation video: PowerTag E installation

Supported mounting positions

Resi9

Mounting position Smart Tag Model number

Top or Bottom

PowerTag Energy R9 M63 1PW

R9M20

Top or Bottom

PowerTag Energy R9 M63 3P

R9M40

Top

PowerTag Energy R9 M63 3PN

R9M41

Top or Bottom

PowerTag Energy R9 F63 1PN

R9M60

Top or Bottom

PowerTag Energy R9 F63 3PN

R9M70

Top

PowerTag Energy R9 M63 1PN

R9M21

Bottom

PowerTag Energy R9 M63 1PN

R9M22

Bottom

PowerTag Energy R9 M63 3PN

R9M42

Top or Bottom

PowerTag Energy R9 M63 3P

R9M43

Acti9

Mounting position Smart Tag Model number

Top or Bottom

PowerTag Energy A9 M63 1P

A9MEM1520

Top

PowerTag Energy A9 M63 1PN

A9MEM1521

Bottom

PowerTag Energy A9 M63 1PN

A9MEM1522

Top or Bottom

PowerTag Energy A9 M63 3P

A9MEM1540

Top

PowerTag Energy A9 M63 3PN

A9MEM1541

Bottom

PowerTag Energy A9 M63 3PN

A9MEM1542

Top or Bottom

PowerTag Energy A9 M63 3P

A9MEM1543

Top or Bottom

PowerTag Energy A9 F63 1PN

A9MEM1560

Top

PowerTag Energy A9 P63 1PN

A9MEM1561

Bottom

PowerTag Energy A9 P63 1PN

A9MEM1562

Bottom

PowerTag Energy A9 P63 1PN

A9MEM1563

Top or Bottom

PowerTag Energy A9 F63 3PN

A9MEM1570

Top

PowerTag Energy A9 P63 3PN

A9MEM1571

Bottom

PowerTag Energy A9 P63 3PN

A9MEM1572

Top or Bottom

PowerTag Energy A9 F63 3P

A9MEM1573

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?