DUG_Connected Thermostat 16 A, ZB_WH-03

Installing the device


Selecting the installation site:

In order for the thermostat to be operated, the internal temperature sensor must be protected as far as possible against external influences and temperature fluctuations. This helps to guarantee reliable detection of the room temperature.
The following should therefore be taken into account when considering the installation site:

  • Minimum installation height: 1.5 m above the floor.

  • Do not install too close to windows, doors or ventilation openings.

  • Do not install above heaters or other heat sources.

  • Do not cover or install behind curtains.

  • Avoid direct sunlight and light from lamps.

  • Do not install in power strips above or next to components that produce heat, such as dimmers or electronic switches.

  • Mounting on the cavity wall requires proper sealing of the conduit box or installation tube, to prevent airflow from affecting temperature sensor performance.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?