LED Indications
Pairing the device
Presetting the device
Status |
User Interaction |
Description |
Enter preset selection |
The thermostat matrix display flashes "P1" when the thermostat is first powered on or after a factory reset to indicate preset “P1" is selected. |
|
Modify preset selection |
The thermostat matrix display flashes P2..P6 when the thermostat rotary push-button is turned. Note: When the thermostat rotary push-button is turned clockwise, the preset increases by one; similarly, the preset decreases by one when the rotary push-button turned anti-clockwise. For more information, refer to the section Presetting the device. |
Setting a sensor type
Resetting the device
Status |
User Interaction |
Description |
Soft reset |
A solid "Sr" LED is displayed on the thermostat matrix display until the user releases the rotary push-button, then "Sr" flashes. For more information, refer to the section Resetting the device. |
|
Factory reset |
A solid "Fr" LED is displayed on the thermostat matrix display until the user releases the rotary push-button, then "Fr" flashes. For more information, refer to the section Resetting the device. |
Showing demand - temperature control modes
Status |
User Interaction |
Description |
Heating demand |
The matrix display a solid red LED to indicate the thermostat is heating when the setpoint is higher than the current room temperature. NOTE: Heating input has been activated.
|
Away mode
Status |
User Interaction |
Description |
Away mode is set in Wiser Home app. |
A dot-matrix display glows, indicates that the thermostat
is in away mode. |
Temperature display
Status |
User Interaction |
Description |
Temperature below minimum display
value |
Note: The thermostat matrix displays temperature limits -9 °C to 99 °C. The thermostat matrix display flashes “--” When the temperature is below -9 degrees. OR The thermostat matrix display flashes “--” when the thermostat cannot determine the temperature due to an error. |
|
Temperature above maximum display value |
Note: The thermostat matrix displays temperature limits -9 °C to 99 °C. The thermostat matrix display flashes “+ +” when the temperature is above 99 degrees. |