DUG_Wiser Plug_WH-08

Pairing the device with the Wiser Hub

Using the Wiser Home app, pair your Plug with the Wiser Hub to access and control the Plug.
To pair the Plug:
  1. On the Home screen, tap .
  2. Tap Devices > and tap Appliances > Smart Plug > Next.
    TIP: The next screen shows the joining process of the Plug.
  3. Press the Plug top push-button fast three times.
  4. Wait for a few seconds until Plug is successfully joined.
  5. Once the device is joined, tap (A) and select an icon suitable for your load and tap Save.
    NOTE: Electric plug icon is assigned by default.
  6. Tap (B) and assign a name.
  7. Tap Next to assign the Plug to an existing room or a new room.
  8. Tap Submit.
You can see the added Plug on the Control tab under the room tab or under ALL devices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?