Shutter
-
On the Home page, tap
.
-
Tap Device Details screen.
to
locate to
A
Device Name: Tap to change the name of the device.
B
Location: Tap to assign the shutter to any room (such as living room, bedroom, kitchen etc). Refer to Setting the device location for more details on how to set the location.
C
Device Type: Tap to change the device type according to your need. Refer to Selecting device type for detailed information on each options.
D
Open duration and Close duration: Tap to set the default run time to open/close the shutter. Refer to Setting the default run time for detailed information.
E
Identify: Tap to identify the device.
NOTE:-
The status LED blinks red and the shutter opens/closes gradually, upon successful identification of the 1-gang shutter or shutter slat.
-
The 1-gang shutter LED will continue to flash until you tap OK.
F
Delete: Tap to remove the device from the system.
G
Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device.
-