DUG_Micro Module Light Switch_WH-04

Resetting the device in Quick Home Connect

It is necessary to reset the devices in the following scenarios:

  • Unpair the device in Quick Home Connect:

    When reset is done successfully. The Wireless switch and device returns to factory default.

  • Integrating into Wiser System

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?