Heat report
The performance of your heating system can be monitored with the Heat Report.
It enables the viewing of historical room, set (target), outdoor temperatures and allows for room-by room comparison over time, to ensure that the system performs according to scheduled and manual operations.
Wiser records room, set and outdoor temperatures on a continual basis and makes the data available in the Heat Report. The report is updated daily and a given day’s temperature data is available the next day. It is possible to view the report on the basis of day, week and month.
To navigate to the Heat report:
Single-room view
When accessed for the first time, the report opens from the single-room view.
This view defaults to display today’s room temperature for the first room, as it appears on the Home screen of the app. It also displays the set temperature for the room (always illustrated by a black line).
The outdoor temperature is not displayed by default, but you can choose to view it by selecting it from room selector.
When viewing a single room, it is possible to see how long it takes for the room to heat up or cool down to the set temperature; the black line shows the set (target) temperature, i.e. Wiser’s heating schedule for the room (if in Auto mode) or the manually selected set temperature (if in Manual mode). This line indicates the room temperature that Wiser is regulating to at all times.
Multi-room view
The multi-room view allows for simultaneous viewing and comparing of up to 16 rooms. The outdoor temperature can also be selected/ deselected in this view.
Monthly view
The monthly view provides a summary of room temperature fluctuations during a given calendar month. All daily temperatures in this view are averaged out due to the screen size.
The outdoor temperature in this view is displayed as a green band indicating the daily min/max temperatures and the range in which the daily temperatures have fluctuated throughout the month.
Temperature Display
The room name and temperature will appear when a temperature line is tapped. Any area outside the line can be tapped to make them disappear again. It is possible to tap on any point of a temperature line, including the outline of the green outdoor temperature area. Temperature lines can be tapped in all three views (Day/Week/Month).
Missing Temperature Data
Temperature data may be missing from the system at times. This could be due to power failures, no internet connectivity, flat device batteries or poor RF signal. Missing data is denoted by a dotted line connecting the two points between which data is unavailable.
If data is missing
for a given date or date range, the question mark on the ROOMS bar
is replaced by . If data for the
date/ range becomes available at a later time, or if the view is changed
to another date/range, with no missing data, the question mark will
reappear.