DUG_Push-button Module, 1-gang/2-gang_WH-04

Selecting device type

Using the Wiser Home app, you can change the device type according to your need.
NOTE: The device type was selected as Shutter when pairing with the Wiser Hub. You can change the device type as Shutter with tilting slats if it has a tilt function.
  1. On the Home page, tap .
  2. Tap Devices > Shutters .
  3. Tap (A) and select a device type.
  4. If the device type is selected as Shutter with tilting slats , tap (B) and select a slat type (C).
  5. Tap Set.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?