DUG_PowerTag-E_WH-09

Enabling Personalized Energy Insights

Using the Wiser Home appWiser appELKO Smart app you can enable Personalized Energy Insights to monitor the energy breakdown, and comparison between similar homes and also view energy-saving tips.
IMPORTANT: To enable Personalized Energy Insights you must meet the following condition:
  • User should be registered in the Europe data center.

  • Users home location must be Sweden.

  • One PowerTag Smart Tag should be configured as Grid (main incomer).

IMPORTANT: To enable Personalized Energy Insights you must configure one PowerTag as Grid (main incomer).
NOTE:
  • You will be notified that this feature is available after PowerTag is commissioned.

  • You can enable this feature and create your home profile.

  • You should have minimum of 1 month of load consumption data to view your energy breakdown. A push-notification will be sent to the user when data is available.

To enable Personalized Energy Insights:

  1. On the Home screen, tap Energy Dashboard > Insights, then tap splash screen (A).

    NOTE: Do not accidentally close the splash screen as it takes 3 weeks for this option to reappear, until that you cannot enable to Personalized Energy Insights.Do not accidentally close the splash screen as it will take 2 weeks and a final reminder after 6 weeks to reappear.
  2. Read the tutorial information and tap Next twice, then tap Unlock Personalized Energy InsightsUnlock Energy Insights.
  3. Read the privacy notice and tap Activate on each page.
    NOTE: Accepting consent is optional.
  4. Once Personalized Energy Insights is successfully enabled, you will receive an in-app notification and then immediately you will be prompted to create a home profile. Refer Creating home profileCreating home profile.
    NOTE: You can also navigate through in-app notification which is received after enabling Personalized Energy Insights by tapping .
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?