DUG_Micro Module Light Switch_WH-04

Testing the device

Before using the puck, manually test the puck and make sure that it works when connected to the devices.

WARNING
HAZARD OF ELECTRIC SHOCK
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Short press the test button once, the connected device turns on/off.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?