DUG_PowerTag-E_WH-08

Triggering notifications and alarms

Using Wiser Home app, you can set alarms to notify overconsumption or no consumption of loads.
NOTE: Each device can have one overconsumption and one no consumption alarm.
To configure alarms:
  1. On Home screen, tap .
  2. Tap Account > Notifications and Alarms.
  3. Tap Create a new alarm (A) and select an alarm type (B).
  4. Select a device from the list (C) and tap Next.
  5. Enable the toggle switch (D) to set the alarm.
  6. Tap (Watts) and enter a value to set a power limit.
  7. Tap (During), select a time limit and tap Set (E).
  8. Tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?