Troubleshooting
Symptom |
Possible cause |
Solution |
---|---|---|
Thermostat temperature measurement is not accurate. |
Check the installation location for possible air flow in conduit box or installation tube. |
Make sure there is proper sealing of the conduit box or installation tube, to prevent airflow from affecting sensor performance. |
The thermostat has gone offline. |
|
|
Unable to join to the Wiser Hub (blinking red LED) |
Poor signal between the Wiser Hub and thermostat. The devices have no power (Thermostat/ Wiser Hub/Wi-Fi® network). |
|
Status | User Interaction | Description |
Unable to set the room temperature by the app. |
Wiser Hub signal is weak or not connected to the Wi-Fi® network. |
Check for a Wi-Fi® signal. |
Find and Bind |
When the user
press and holds the rotary push-button for >8s, "Fb" LED is displayed
on the thermostat matrix display. |
|
“X” mark is displayed on LED matrix |
Device is lock and LED matrix displays “X” |
Press rotary push-button for > 5 s to exit the menu. |