DUG_Micro Module Light Switch_WH-04

Troubleshooting in Quick Home Connect

Symptom

Possible cause

Solution

LED displays amber in Puck (Micro module light switch).

Pairing not completed and returned to factory reset.

Pair the Wireless switch and the device again. Refer to Pairing Wireless switch with Micro module light switch,

Wireless switch not able to control the device reliably.

The Wireless switch and the device are too far away from each other.

Place the Wireless switch in a position closer to the device.

The Wireless switch lost pairing.

Pair the device again

The Wireless switch battery is discharged.

Replace the battery of the Wireless switch.

Scenario

Procedure

Control multiple devices with one Wireless switch.

To centralize control with one Wireless switch, first pair it with already connected devices. Then, pair the new device to existing group/network.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?