System User Guide Wiser Home (France) - 10

Status bar on Home Screen

You can set whether to display the Grid Status on the Home Screen.

On the Home Screen settings, tap the slider (A) to enable / disable the status bar.

NOTE: Disabling the Status Bar on the Home Screen will also disable access to the grid status forecast, gestures and eco tips. Eco tips can be accessed by tapping an EcoWatt notification.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?