System User Guide Wiser Home (France) - 10

EcoWatt

EcoWatt informs you about the state of the national power-grid and offers a forecast of the expected tension in the national power grid.

EcoWatt provides information on eco-gestures that can help relieve the burden on the national electricity grid.

Features:

  • Shows the state of the power grid.

  • Sends notifications about the state of the power grid.

  • Sends alerts if there is a risk of power cuts.

  • Provides eco-gestures to help relieve grid tension.

When enabled, EcoWatt will display the status of the power grid (A) on the Home Screen.

Color Text Recommended actions
Green National Electrical Grid is operating normally The power grid is not under much tension. Eco-gestures are generally recommended to help safe energy and money.
Amber National Electrical Grid is tensed The power grid is stressed. Eco-gestures are recommended to help relieve the tension..
Red National Electrical Grid is very tensed The power grid is critical. Eco-gestures are highly recommended to help prevent power outages.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?