System User Guide Wiser Home (France) - 10

Insights

The Insights provides information on the annual bill for the tariff set. It helps to keep track of your energy.

NOTE: The option to set a tariff is only available if you have an Energy device installed in your home. For more information, please refer to the Device User Guide of the respective device.

  1. For a more detailed overview, tap Energy costs (A).

    Energy-Insight without Heating Devices:

    Energy-Insight with Heating Devices

    Tap banner (B) to enable Reduce My Bill with Artificial Intelligence (RMB - AI). RMB - AIis a feature that allows users to reduce electricity costs by enrolling high energy devices like EV Charger (EVlink Home Smart, Schneider Charge, EVlink socket) or resistive Water boilers (controlled with a Wiser Power Micromodule). It is used with variable tariffs, such as peak/off-peak tariff, and relies on users to answer routine questions. Refer to respective device user guide for detailed information on the Reduce my Bill service.

    NOTE: If you have installed and configured solar panels in your home, RMB - AI could save up to 50% on your electricity bill.

  2. You can change the displayed timeframe (hours, days, months and years).

    IMPORTANT: If you have installed PowerTag on solar or solar with battery My savings is available to view savings and earning history.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?