Operating Elements
A | Setup |
Activates the temporary Wi-Fi® network of the Hub. Useful for troubleshooting. |
B | Heating Override* |
Turning on the heating override will turn on the connected heating system for 2 hours regardless of any settings in the app or thermostats. In this state the boiler will self regulate its temperature. To start override: press and hold button for more than 3 seconds. To stop override, short press the button. This will put the heating back under system control. |
C | Hot Water override |
Turning on the Hot Water override will turn on the connected Hot Water for 1 hour. In this state the hot water will be regulated by a thermostat or the boiler. To start override: press and hold button for more than 3 seconds. To stop override, short press the button. This will put the hot water back under system control. |