SUG_Wiser_Home_UK_IRL_WH-00

Resetting to factory defaults

You can reset the Hub to it’s factory defaults.

NOTE: Resetting the Hub will delete the Wiser System you have set up. If you want to reinstall your System, you will have to also reset all your Connected Devices and add them again to your System. Refer to resetting the device chapter in the Device User Guide of the respective Device. List of Wiser Devices provides the links to Device user guide for each devices. You will have to recreate all schedules, moments, automations, etc.

Only use the reset when you want to decommission your Wiser System or if all other troubleshooting measures failed.

To reset the Hub to factory defaults:

  1. Press and hold the Setup button (A) until the Setup LED turns solid red followed by all LEDs flashing red once.

This indicates that the hub is successfully reset.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?