DUG_Power_Micromodule_WH-04

Reduce My Bill in Wiser Home

The Reduce My Bill feature automatically schedules your high-consuming devices to run during the cheapest electricity rates, helping to lower your energy bill. By enrolling devices like EV chargers or resistive water boilers, this feature shifts loads to low-tariff periods. It works with variable tariffs, such as peak/off-peak rates, and requires users to answer routine questions.

For more information on Reduce My Bill refer to the respective System User Guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?