DUG_Smoke alarm DC_WH-02

Changing the device location

Using the Wiser Home app, you can change the device location.
To change the device location:
  1. On the Home page, tap .
  2. Tap Devices > Smoke Alarm > Location (A) for any of the following:
    • To create a new room, enter the room name (B) and tap Submit.
    • Change the device location (C).
    NOTE: To remove the device from the room, tap Remove from Room (D).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?