DUG_Water Leakage Sensor_WHP-01

Setting device notification

Using the Wiser Home app, you can enable or disable the sensor notification.
To enable or disable the sensor notification:
  1. On the Home page, tap .
  2. Tap Devices > Water Leakage Sensor > Notify me if leak is detected (A) to enable or disable the sensor notification toggle switch.
    TIP: Additionally, you can enable or disable the sensor notification toggle switch by tapping on the Home page Water Leakage Sensor > Device settings > Notify me if leak is detected (A).
    NOTE:
    • Sensor notification toggle switch (A) is OFF by default.

    • Notifications created via automation are treated as separate notifications.

    • When the sensor detects water, it sends a notification and a sound alarm, and the alarm continues until the sensor is removed from the water.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?