0100CT2302

Servicing the Microgrid

In addition to a wide offer of technology and products, Schneider Electric provides the following services which can be customized to your needs, helping you realize the full value microgrids bring to your business.

Engineering Services

Our Packaged Consulting Services include:

  • Microgrid Feasibility Study: The first step in determining if a new or existing site can support a microgrid. It includes load analysis, size onsite generation and storage assets and preliminary pricing and financial services.

  • Microgrid Front End Engineering Design: A detailed design to get more accurate pricing, layout, and implementation plan.

  • Microgrid Complete Design Package: 100% design package including Schneider Electric serving as the Engineer of Record. Designed for optimal system operation and total cost of ownership.

Schneider Electric can also provide following standalone consulting services:

  • Microgrid Site Audit and Electrical Assessment

  • Microgrid Design Assurance/Assistance

  • Battery Loading Analysis

  • Utility Interconnect Support

  • Short-Circuit, Coordination and Arc Flash Study (SCCAF Study)

  • Power Quality and Harmonic Analysis

  • Power System Transient Analysis

Startup Services

Schneider Electric field service technician(s) will perform visual, mechanical, and electrical tests on the switchboard. Schneider Electric provides a 12-month warranty extension to equipment that is successfully tested and started-up by Schneider Electric.

Recurring Service Plans

Recurring Service Plans

Schneider Electric has three standard service packages to choose from for Flex.

  • Essential—Essential Service Plan is required for all EcoStruxure Microgrid Flex projects. It includes Remote Troubleshooting and Diagnostics by microgrid engineers.

  • Advanced and Plus Advanced—Advanced and Plus Advanced are the recommended service plan packages for all projects. They are for three years of coverage. They can be added on via the selector at the same time as the initial purchase of EcoStruxure Microgrid Flex or added in the future.

Service Plans start as soon as the system is operational.

A service plan is more than a warranty because it includes proactive, fast, system-level support by specialists.

Service Plan Packages

Features

Essential

Advanced

Plus Advanced

Support to Operations

Troubleshooting and Diagnostics

Direct Access to Microgrid Technical Experts (Business Hours) – Phone and Email

Emergency Support

Break-fix on-site intervention:

Services Level Agreement - max 8H*

Optional*

On-site intervention labor coverage

Parts

Repair Parts

Parts coverage for remedial repairs for
Schneider Electric assets

Spare Parts

Spare parts purchased and stored on-site available for immediate use Discount Discount

On-site Maintenance

Sequence of Operations Test

System functional testing to confirm operation of software, controls, and assets Optional Optional

Preventative Maintenance

Annual inspection and testing of electrical distribution equipment plus one cycle of de-energized preventative maintenance

Microgrid Service Feature Summary

1. Support to Operations

  • Troubleshooting and Diagnostics: Fast and effective troubleshooting starts by having a si ngle point of contact that you can reach directly by phone or email that understands the system. Microgrid Support Engineers in our Connected Services Hub will remotely provide quick response time, troubleshoot, and dispatch correct resources to the site (if needed).

  • Emergency Support: Onsite Intervention for Reactive Unplanned Events

    • All onsite labor and travel are covered for emergency and other non-preventative maintenance work providing extended warranty coverage.

    • Receive priority access to personnel with service plan in place.

    • Schneider Electric Field Services Representative dispatched to site 24/7

    • Options for 4 or 8 hour guaranteed onsite response time, if site is located within 100 miles of a Schneider Electric Service location

2. Parts

  • Repair Parts: With a service plan that includes preventative maintenance, you can have all replacement parts used for remedial repairs covered by Schneider Electric. You will not have to pay any extra costs to fix equipment and restore full operations.

  • Spare Parts: Spare parts are field installable components or parts for any new and existing equipment.

3. On-site Maintenance

  • Sequence of Operations Test: Ensures islanding capability is functional and meets operational intent. The Schneider Electric engineer onsite runs the microgrid system through its programmed sequence of operations, which includes a report outlining results and recommendations.

  • Preventative Maintenance: Having a strategy of planned preventative maintenance mitigates unplanned downtime.

    • Annual Energized Diagnostic: Provides early warning signs of equipment failure without interrupting operations. It includes infrared scanning, transformer oil sampling, and visual inspections.

    • De-Energized Maintenance: Completed once every three years, these services provide comprehensive maintenance in support of your facilities schedule, this includes overcurrent protective device testing, cleaning, and lubrication to meet specification and electrical testing including insulation and current path.

References Description Line Code Description
SRVRECMGFLEX1_E Microgrid Flex Service Plan Essential. Remote Troubleshooting and Diagnostics. For 3 section 3000a ECC, 1 year coverage Operate and Maintain Microgrid
SRVRECMGFLEX1_A Microgrid Flex Service Plan Advanced.
For 3 section 3000a ECC. 3-year plan.
SRVRECMGFLEX1_PA Microgrid Flex Service Plan Plus Advanced.
For 3 section 3000a ECC. 3-year plan.
SRVRECMGRECSOOFLEX Microgrid sequence of Operations Test. Once a year for 3 years.
Part or recurring service plan. Onsite work
SRVRECMGEMER_8FLEX Microgrid Emergency Response Time—8 hours for Flex Service.
Add-on for SLA of 8 hours onsite
SRVINCMGLVMV_FLEX1 Startup for Microgrid Equipment for 3000a 3 section ECC. One site visit Startup Microgrid
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?