Before You Begin
Before performing any of the tasks listed in the table starting, you must be familiar with and follow the requirements contained within NFPA 70E: Standard for Electrical Safety in the Workplace or CSA Z462: Workplace Electrical Safety. In addition, all electrical equipment must be installed in accordance with local and national installation codes and adequately maintained per NFPA 70B: Recommended Practice for Electrical Equipment Maintenance and instructions from Schneider Electric. Failure to follow the safety recommendations can result in death or serious injury, as well as property damage.
Square D equipment manufactured by Schneider Electric is designed, built, and tested to comply with industry standards, including but not limited to the following standards:
-
C37.20.1, IEEE Standard for Metal-Enclosed Low-Voltage Power Circuit Breaker Switchgear
-
C37.20.2, IEEE Standard for Metal-Clad Switchgear
-
C37.20.3, IEEE Standard for Metal-Enclosed Interrupter Switchgear
-
C37.20.7, IEEE Guide for Testing Metal-Enclosed Switchgear Rated Up to 38 kV for Internal Arcing Faults
-
UL 67, Panelboards
-
UL 98, Enclosed and Dead-Front Switches
-
UL 845, Motor Control Centers
-
UL 891, Switchboards
With the exception of C37.20.7, these standards do not require that equipment be tested for internal arcing faults. Schneider Electric's position is to de-energize equipment to establish an electrically safe work condition prior to working on or inside the equipment. Always follow safety precautions.
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
DANGER