0110DB9901 R04/20

The NEC Rules

Equipment Rated for 100 A or Less — NEC 110.14(C)(1)(a) items 1 through 4

NOTE: The equipment sizes and ampacities shown in the figures are arbitrary. The rules apply to any equipment rated 100 A or less.

For equipment with termination provisions for circuits rated 100 A or less or marked for 14 AWG through 1 AWG conductors, the NEC allows conductors to be used based on the following four conditions:

  1. Conductors rated 60°C (see Conductors Rated 60 °C).

  2. Conductors with higher temperature ratings, provided the ampacity is determined based on the 60°C ampacity of the conductor (see Conductors with Higher Temperature Ratings).

  3. Conductors with higher temperature ratings, provided the equipment is listed and identified for use with such conductors (see Conductors with Higher Temperature Ratings).

  4. Conductors for specific motor applications (see Conductors for Specific Motor Applications). This permission is specific to Design B, C, or D motors because those motors are temperature evaluated with conductors based on 75°C ampacity.

Conductors Rated 60 °C

Conductors with Higher Temperature Ratings

Conductors with Higher Temperature Ratings

Conductors for Specific Motor Applications

Equipment Rated above 100 A — NEC 110.14(C)(1)(b) items 1 and 2

For equipment with termination provisions for circuits rated above 100 A or marked for conductors larger than 1 AWG, the NEC 110.14(C)(1)(b) items 1 and 2 allow conductors to be used based on the following conditions:

  1. Conductors rated 75°C (see Conductors Rated 75°C).

    Conductors Rated 75°C

  2. Conductors with higher than 75°C ratings provided the conductor ampacity does not exceed the 75°C ampacity of the conductor size used (see Conductors with Higher Temperature Ratings). This condition also permits the conductors to be used at ampacities higher than 75°C if the equipment is listed and identified for the higher rating. However, for equipment rated 600 V and less, the vast majority of equipment termination ratings are 75°C.

    Conductors with Higher Temperature Ratings

The equipment termination ratings versus conductor insulation ratings are summarized in Conductor Insulation Versus Equipment Termination Ratings.

Conductor Insulation Versus Equipment Termination Ratings

Termination Rating (°C)

Conductor Insulation Rating

60°C

75°C

90°C

60 OK OK (at 60°C ampacity) OK (at 60°C ampacity)
75 No OK (at 60 or 75°C ampacity) OK (at 60 or 75°C ampacity)
60 / 75 OK OK (at 60 or 75°C ampacity) OK (at 60 or 75°C ampacity)
90 No No OK*

Caution on Using Lug Ratings

When terminations are inside equipment such as panelboards, motor control centers, switchboards, enclosed circuit breakers, safety switches, etc., follow the temperature rating identified on the equipment labeling instead of the rating of the lug itself. Manufacturers commonly use 90°C-rated lugs (i.e., marked AL9CU) on equipment rated only 60°C or 75°C. The use of the 90°C-rated lug in this type of equipment does not allow the installer to use 90°C wire at the 90°C ampacity. The Underwriters Laboratories® General Information on Electrical Equipment Directory states the following about terminations: “A 75°C or 90°C temperature marking on a terminal (e.g., AL7, CU7AL, AL7CU or AL9, CU9AL, AL9CU) does not in itself indicate that a 75°C or 90°C insulated wire can be used unless the equipment in which the terminals are installed is marked for 75°C or 90°C.”

Review the labeling of all devices and equipment for installation guidelines and possible restrictions.

Available Equipment Terminations

Remember that a conductor has two ends, and that the termination on each end must be considered when applying the sizing rules. For example, consider a conductor wired to a 75°C termination on a circuit breaker at one end, and a 60°C termination on a receptacle at the other end. This circuit must be wired with a conductor that has an insulation rating of at least 75°C (due to the circuit breaker) and sized based on the ampacity of 60°C (due to the receptacle).

For electrical equipment rated for 600 V and less, terminations are typically rated at 60°C, 75°C or 60/75°C. No distribution or utilization equipment is listed and identified for the use of 90°C wire at its 90°C ampacity. This includes distribution equipment, wiring devices, transformers, motor control devices, and even utilization equipment such as HVAC, motors, and light fixtures. Installers and designers who have not realized this fact have equipment that does not comply with the National Electrical Code and that has been turned down by the electrical inspector.

In equipment rated over 600 V, the effect of the conductor as a heat sink is minimized, and ratings higher than 75°C are available. NEC 110.40 recognizes that conductors with sizes based on the 90°C ampacity can be used in installations over 600 V.

An example of how 90°C wire might be used at its 90°C ampacity is shown in 90°C Wire Used at 90°C Ampacity. Note that the conductor does not terminate directly in the distribution equipment, but in a terminal or tap box using 90°C-rated terminations.

90°C Wire Used at 90°C Ampacity

Frequently, manufacturers are asked when distribution equipment will be available with terminations that will permit 90°C conductors at the 90°C ampacity. This would require not only significant equipment redesign (to handle the additional heat), but also coordination of the downstream equipment where the other end of the conductor terminates. Significant changes in the product testing/listing standards also would have to occur.

A final note about equipment: some equipment requires the conductors that are terminated in the equipment to have an insulation rating of 90°C, but an ampacity based on 75°C or 60°C. This type of equipment might include 100% rated circuit breakers, fluorescent lighting fixtures, etc., and is marked to indicate such a requirement. Check with the manufacturer of the equipment to see if you need to take into account any special considerations.

What About Higher-Rated Conductors and Derating Factors?

One advantage to conductors with higher insulation ratings is noted when derating factors are applied. This advantage is noted in the last sentence of NEC 110.14(C): “Conductors with temperature ratings higher than specified for terminations shall be permitted to be used for ampacity adjustment, correction, or both.” Derating factors may be required because of the number of conductors in a conduit, higher ambient temperatures, or internal design requirements for a facility. By beginning the derating process at the ampacity of the conductor based on the higher insulation value, you may not be required to upsize the conductor to compensate for the derating.

Remember these points while studying the derating process example:

  • The ampacity value determined after applying the derating factors must be equal to or less than the ampacity of the conductor based on the temperature limitations at its terminations.

  • The derated ampacity becomes the allowable ampacity of the conductor, and the conductor must be protected against overcurrent in accordance with this allowable ampacity.

Example of Derating Process

Assume that you have a 480Y/277 Vac, 3-phase, 4-wire feeder circuit to a panelboard supplying 200 A of noncontinuous fluorescent lighting load. Assume that the conductors will be in a 40°C ambient temperature and the conductors originate and terminate in equipment with 75°C terminations.

Additional information to consider from the NEC:

  • Since the phase and neutral conductors all will be in the same conduit, consider the issue of conduit fill. NEC 310.15(E)(3) states that the neutral must be considered to be a current-carrying conductor since a major portion of the load is a nonlinear load (electric discharge lighting).

  • Based on this, four current-carrying conductors will be in the raceway. NEC 310.15(C)(1) requires a 20% reduction in the conductor ampacity based on having four to six current-carrying conductors in the raceway.

  • According to the ambient correction factors in Table 310.15(1), an adjustment must be made of 0.88 for 75°C and 0.91 for 90°C.

Calculate, using a 75°C conductor such as THWN:

300 kcmil copper has a 75°C ampacity of 285 A.

Using the factors noted earlier: 285 A x 0.80 x 0.88 = 201 A

201 A is now the allowable ampacity of the 300 kcmil copper conductor for this circuit. Had the derating factors for conduit fill and ambient not been required, a 3/0 copper conductor would have met the needs for this application.

Calculate, using a 90°C conductor such as THHN:

250 kcmil copper has a 90°C ampacity of 290 A.

Using the factors noted earlier: 290 x 0.80 x 0.91 = 211 A

211 A is less than 75°C ampacity of a 250 kcmil copper conductor (255 A), so the 211 A would now be the allowable ampacity of the 250 kcmil conductor. Had the calculation resulted in a number larger than the 75°C ampacity, the actual 75°C ampacity would have been used as the allowable ampacity of the conductor. This is critical since the terminations are rated at 75°C. Note that the conductor size was reduced by one size (300 kcmil to 250 kcmil) and still accommodated all of the required derating factors for the circuit. This is the primary advantage of using
90°C conductors.

Therefore, when using 90°C wire for derating purposes, you can begin derating at the 90°C ampacity. You must compare the result of the calculation to the ampacity of the conductor based on the termination rating (60°C or 75°C). The smaller of the two numbers then becomes the allowable ampacity of the conductor.

Use of Other Than Table 310.16

The default rule for conductors which enter an enclosure is Table 310.16, unless listed and marked otherwise. The other tables, such as 310.17, may apply to a conductor while it is in free air, but the smaller number of 310.16 still applies at the point of termination in equipment. If a high ambient derating factor is applied, a larger conductor may be required. The equipment is provided with a standard size and quantity of terminations in alignment with Table 310.16 and a user must specify if other terminations are required for the particular situation.

Number of Conductors Per Terminal

The NEC contains some key references regarding how many conductors can be terminated in a single terminal. NEC 110.14(A) has a blanket statement requiring that terminals for more than one conductor shall be so identified. This would mean that the terminal (or terminal bar) would have to be identified to accept more than one conductor. For equipment that contains a terminal or terminal bar, this identification is generally found on the wiring diagram or some other label on or inside the product.

There is some confusion regarding equipment grounding conductors, and grounded conductors. The NEC only allows multiple grounded conductors in one terminal when the conductors are paralleled in the same circuit, and the terminal is identified for multiple conductors. Equipment grounding conductors from different circuits can be grouped in terminals to the limit of the terminal identification.

Summary

Proper termination of conductors is a critical part of having a safe electrical installation. Assigning the ampacity of a conductor is impacted by not only the physical characteristics of the conductor, but the connected equipment as well. Closely adhering to the NEC rules will not only avoid rejected installations from inspectors, but will help to avoid having problems with the terminations in the future.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.