0600DB1901

Additional Information

https://www.schneider-electric.us/en/download

Square D™ field testing and maintenance guides, available in the download center, contain typical watts loss data to be used for heat generation estimates. Resistance can be calculated from the watts loss data if desired, but for reasons noted above, Schneider Electric does not recommend using these values to determine the usability of a circuit breaker.

“Circuit Breaker Operating Temperatures”, document number 0600DB1603, describes the acceptable operating temperature of a circuit breaker as defined by the UL489 standard.

For more information concerning Square D brand low voltage circuit breakers, refer to the appropriate product catalog. These catalogs contain general and detailed information on circuit breaker characteristics, accessories, wiring diagrams, and trip curves.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.