0600IB1201

Section 4—Performance Tests for PowerPacT Circuit Breakers

These tests check the performance of PowerPacT electronic trip circuit breakers.

Performance Tests

DANGER
Hazard of Electric Shock, explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E or CSA Z462.
  • This equipment must be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors and covers before turning on power to this equipment.
  • Do not touch the circuit breaker terminals or the test leads while the circuit breaker is being tested.
Failure to follow these instructions will result in death or serious injury.

Do the performance tests in the order given to maximize the accuracy of the test results.

NOTE: Never do the contact resistance test before doing the instantaneous primary injection testing. The primary injection testing will ensure the contacts are clear of resistive films, oxidation and foreign material.

The following tests are intended to verify that a circuit breaker is operating properly. Precisely controlled factory testing conditions are used to establish the characteristic trip curves. If field test results fall outside the characteristic trip curve tolerance band, carefully evaluate the test conditions and methods for accuracy.

When questionable conditions or results are observed during inspection and performance tests, consult your local field sales office. Circuit breakers with accessories or factory modifications may require special investigation. If it is necessary to return a circuit breaker to the manufacturing facility, use proper packaging and packing materials to avoid shipping damage.

Insulation Resistance Test (Dielectric Testing)

NOTICE
Hazard of Equipment Damage
  • Insulation resistance testing (dielectric tests) may damage MicroLogic 5.0/6.0P or 5.0/6.0H trip units.
  • Remove rating plug from trip unit prior to testing.
  • Replace trip unit if rating plug was not removed during tests or if trip unit was exposed to more than 700 Vac.
Failure to follow these instructions can result in equipment damage.

Severe environmental conditions can reduce the dielectric strength of molded case circuit breakers. Check insulation resistance during electrical system testing. To check the insulation resistance, perform the following steps:

  1. De-energize and isolate the circuit breaker.

  2. Clean the circuit breaker as described earlier.

  3. Using a megohmmeter with a capacity of 500 -1000 Vdc, apply voltage from: a. Each phase-to-ground with the circuit breaker on (circuit breaker contacts closed). b. Phase-to-phase with the circuit breaker on (circuit breaker contacts closed). c. Between each line and load terminal with the circuit breaker off (circuit breaker contacts open).

  4. Record resistance values. Resistance values of less than one megohm (1,000,000 ohm) should be investigated.

NOTE: 5.2E 5.3E, 6.2E, 6.3E MicroLogic trip units have some normal leakage due to internal circuits for metering. When testing systems with more than 10 circuit breakers with these trip units, it may be necessary to open some of the circuit breakers at a time to make sure all breakers and equpment is sound and insulation resistance is within acceptable limits.

MicroLogic Trip Unit Checks

Circuit breakers with MicroLogic trip units can have their trip unit operation tested with secondary injection testing using the one of the available test kits. (See Section 6—Available Test Equipment for available test kits by circuit breaker.)

Secondary injection testing does not test the current transformers and connections. Primary injection testing can be used to ensure that all trip system connections have been correctly made.

If the circuit breaker is tested by the primary injection method, the PowerLogic™ system can remain connected to the circuit breaker during testing without affecting the results.

NOTE: Testing a circuit breaker connected to a PowerLogic system causes the PowerLogic system to react as if the circuit breaker were experiencing the actual faults.

Procedure to Defeat Zone-Selective Interlocking

Zone-selective interlocking (ZSI) is a method of communication between electronic-trip overcurrent protective devices. ZSI allows interlocked devices at different levels to work together as a system in which a short circuit or ground fault is isolated and cleared with minimum time delay. The purpose of defeating ZSI is to verify the characteristics of the specific circuit breaker short-time and ground-fault trip delay functions.

Secondary Injection

Field installation of a trip unit requires secondary injection testing with a Full-Function Test Kit for PowerPacT P- and R-frame circuit breakers and a UTA for PowerPacT H-, J-, and L-frame circuit breakers. This will ensure that the newly-installed trip unit is functioning properly. The test will require opening and closing the circuit breaker. Follow the procedures outlined in the instruction bulletins shipped with the circuit breaker and the Full-function Test Kit.

  1. Make sure the circuit breaker is isolated from all upstream and downstream devices.

  2. Perform secondary injection testing as outlined in the instruction bulletin shipped with the full-function test kit or UTA. Verify that all applicable trip unit functions are operating properly.

  3. Repeat step 2 with the circuit breaker in the open position.

    NOTE: The test kit states that the circuit breaker should be closed when performing the test. Do not close the circuit breaker for this step.
  4. If any test fails, do not put the circuit breaker into service and contact the local sales office for factory authorization service.

Primary Injection Testing

Primary injection testing can be used to ensure that all trip system connections have been correctly made.

NOTE: Secondary injection testing continues to be the Schneider Electric preferred method for testing circuit breakers. Improper primary injection testing can cause damage to the circuit breakers. Failure to conduct primary injection testing in the proper manner could result in circuit breakers passing testing, while ultimately damaging the integrity of the circuit breaker long term.
NOTICE
Hazard of Equipment Damage
Make connection to the circuit breaker carefully using rated cable and appropriate connection methods. Do not use clamps or other methods that can score or otherwise damage the finish of the connectors.
Failure to follow these instructions can result in equipment damage.
  1. If performing primary injection testing on fixed circuit breakers, connect circuit breaker to power supply using rated cable and appropriate connection method.

  2. Record each of the original trip unit switch settings. (Settings must be reset after testing is complete.)

  3. Set the long-time pickup (Ir) switch (A) to the minimum setting.

    Long-Time Pickup (Ir)

    1. For ground-fault and/or zone-selective interlocked trip units, use the test kit to inhibit ground-fault and zone-selective interlocking functions.

    2. If an auxiliary power supply is being used for the MicroLogic trip unit, disconnect the auxiliary power supply.

    3. Find the primary injection current needed by multiplying the long-time pickup current (long-time pickup setting Ir x sensor plug In) x 125% (i.e. Ir x In x 1.25).

    4. Inject primary current into A-phase and monitor the overload indicator light. Verify that the overload indicator light (A) lights between 105% and 120% of the Ir x In value.

      NOTE: On H-, J-, and L-frame circuit breakers LED:

      The green “Ready” LED (B) blinks slowly when the electronic trip unit is ready to provide protection. It indicates the trip unit is operating correctly.

      Orange overload pre-alarm LED (C): steady on when I > 90% Ir

      Red overload LED (A): steady on when I > 105% Ir

    5. Repeat for all phases and neutral (if applicable).

    6. If overload indicator light does not light correctly, check all trip unit connections and test setup. If unit still fails primary injection testing, contact the local sales office.

      Overload Indicator Light

Circuit Breakers with Integral Ground Fault Protection

MicroLogic electronic-trip circuit breakers with the integral ground-fault protection function require special attention when testing overload and short-circuit functions. The single-pole primary injection tests for the inverse-time overcurrent, short-time and instantaneous functions will cause ground-fault trips due to the return current path not going through the circuit breaker. To overcome this difficulty, use the Hand-Held, Full-Function, or UTA Test Kit to defeat the ground-fault function on PowerPacT circuit breakers equipped with MicroLogic trip units.

Ground-Fault Protection and Indication Only Tests for Radial Systems

DANGER
Hazard of Electric Shock, explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E or CSA Z462.
  • This equipment must be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors and covers before turning on power to this equipment.
Failure to follow these instructions will result in death or serious injury.

Ground-Fault Trip Test

The ground-fault function of a MicroLogic electronic-trip circuit breaker provides ground-fault protection for equipment with adjustable pickup and delay values. the ground-fault delay feature determines how long the circuit breaker waits before initiating a trip signal during a ground fault. Performance of the ground-fault functions of the circuit breaker can be tested using a high-current, low-voltage ac power supply.

Test Procedure

  1. Completely de-energize and remove the circuit breaker from service.

  2. Before testing, record pickup and delay setting for all functions. Reset the trip unit to these same settings after the test procedure is completed.

  3. If testing a circuit breaker that is equipped with zone-selective interlocking, follow the procedure to defeat zone-selective interlocking on Procedure to Defeat Zone-Selective Interlocking. If you are using a secondary injection test kit for these tests, carefully read and follow the test kit instructions about zone-selective interlocking.

    NOTE: Failure to defeat zone-selective interlocking will result in trip time inaccuracy.
  4. Use these settings for the test:

    Long-time Pickup/Ampere Rating = Max.

    Long-time/Overload Delay = Max

    Short-time/Short-circuit Delay = Max. (I2t IN or ON)

    Instantaneous = Max.

    Ground-fault Pickup = Min.

    Ground-fault Delay = 0.2

  5. Follow the hookup procedure appropriate to the test application.

    For circuit breakers without a neutral current transformer, go to step 8.

    For circuit breakers with the integral ground-fault function in a three-phase, four-wire system, an externally-mounted neutral current transformer (CT) must be used. The neutral CT is connected to the circuit breaker by a shielded cable (14 AWG [2.1 mm2] wire is recommended).

    NOTE: When testing, disconnect or turn off 24 Vdc control power to F1 and F2, if equipped and disconnect the Hand-Held or Full-Function Test Kit from the trip unit, if connected.

    Test Hookup Diagram for Neutral CT Phasing Test

    See circuit breaker instructions bulletin for connections to circuit breaker and neutral CT.

    Test Hookup Diagram for Neutral CTSize Test

    See circuit breaker instructions bulletin for connections to circuit breaker and neutral CT.

  6. Verify correct phasing of the neutral CT (three-phase, four-wire systems) by performing a No Trip Test as follows:

    1. Connect the circuit breaker and neutral CT as shown in Test Hookup Diagram for Neutral CT Phasing Test. The jumper must go from the load connection on the circuit breaker to the H1 connection on the neutral CT (or the side of the neutral CT that has the red dot). Connect the secondary of the neutral CT according to the circuit breaker instruction manual or the neutral CT instructions.

    2. Apply current above the ground-fault pickup level and maintain longer than the ground-fault delay.

    3. The circuit breaker must not trip. No trip indicates that both the phase CT and neutral CT are phased properly.

  7. Test Hookup Diagram for Circuit Breaker Without Neutral CT

    Test Hookup Diagram for Ground-Fault Pickup and Delay Test

    Verify the correct size of the neutral CT (three-phase, four-wire systems) by performing a Trip Test as follows:

    1. Connect the circuit breaker and neutral CT as shown in Test Hookup Diagram for Neutral CTSize Test. Connect the polarity (+) terminal of the high current injection unit to the load side of the circuit breaker. The jumper must go from the line connection on the circuit breaker to the H1 connection on the neutral CT (or the side of the neutral CT that has the red dot). Connect the non-polarity (-) terminal of the high current injection unit to H2 on the neutral CT (on the line side of the circuit breaker). Connect the secondary of the neutral CT according to the circuit breaker instruction manual or the neutral CT instructions.

    2. Apply current.

    3. The circuit breaker must trip at half the value of the ground-fault pickup. Tripping indicates that both the phase CT and neutral CT have the same turns ratio (same size).

  8. Test ground fault pickup and delay by performing a trip test as follows:

    1. Connect the circuit breaker as shown in Test Hookup Diagram for Circuit Breaker Without Neutral CT, (three-phase, three-wire systems) or Test Hookup Diagram for Ground-Fault Pickup and Delay Test (three-phase, four-wire systems).

      NOTE: The recommended method of testing ground-fault pickup and delay is the “pulse” method. This method will be the most accurate, but requires that the test equipment have a calibrated image-retaining oscilloscope or high-speed sampling rate digital ammeter. An accurate timer is needed to monitor delay time.
    2. After the circuit is properly connected and closed, apply current in short pulses of 10-cycle duration. Starting at 70% of the expected trip value, increase the current on each succeeding pulse until the circuit breaker trips.

    3. Reclose the circuit breaker and reduce the current level; pulse again to determine if the pickup level found was overshot.

    4. Repeat steps b and c to further isolate the pickup point.

    5. To determine delay time, test each pole of the circuit breaker individually at 150% of the ground-fault pickup setting. Monitor the time from this pickup point until the circuit breaker trips to obtain the delay time.

    6. Record pickup and delay values and compare the results to the trip curve.

The ground-fault test can also be done using secondary injection testing using the Full-Function Test Kit. Secondary injection testing does not test the current transformers and connections.

Contact Resistance Test

Circuit breaker pole resistance tests are not reliable indicators of circuit breaker performance because the resistance values are influenced by a number of transient factors including contact surface oxidation, foreign material between the contacts, and testing methods. NEMA AB 4 paragraph 6.4.1 states: “The millivolt drop of a circuit breaker pole can vary significantly due to inherent variability in the extreme low resistance of the electrical contacts and connectors. Such variations do not necessarily predict unacceptable performance and shall not be used as the sole criteria for determination of acceptability.”

High pole resistance may also be caused by eroded contacts, low contact force, and loose termination. The only one of these factors likely to be present on a new circuit breaker is a loose termination, since the contacts are new and there has been no opportunity for contact pressure to have drifted from the factory setting. A loose termination can be corrected in the field.

If a contact resistance test is done, it is important to do it after the contacts have been conditioned by instantaneous primary injection testing to ensure the contacts are clear of resistive films, oxidation and foreign material. If the circuit breaker has been in service with no performance issues, (overheating or nuisance tripping), contact resistance measurements are redundant and of little value.

Square D recommends that a DLRO (Digital Low Resistance Ohmmeter) be used, using a 10 A dc test current for circuit breaker ratings below 100 A, and using 100 A dc for circuit breakers rated 100 A and above. the median (middle) value of three readings (toggling the circuit breaker between each reading) should be recorded for each pole tested. If this value is equal to or less than the value listed in Maximum Micro-Ohms Per Pole, the pole is acceptable. If the reading is higher, the cause should be investigated and corrected if possible. Contact your local field office for more information.

Maximum Micro-Ohms Per Pole

PowerPacT Micro-Ohms (u ohm)
Type Rating
HD, HG, HJ, HL, HR 60 1,500
100 1,200
150 600
JD, JG, JJ, JL, JR 250 450
LD, LG, LJ, LL, LR 250 630
400 240
600 160
DG, DJ, DL 400 240
600 140
PG, PJ, PK, PL 250 488
400 200
600 114
800 78
1000 55
1200 39
RG, RJ, RK, RL 600 106
800 81
1000 63
1200 53
1600 50
2000 38
2500 33

Remove Test Connections

Upon completing testing:

  • Remove test connections from circuit breaker.

  • Inspect connections for damage caused by testing.

  • Reset the long-time pickup switch to original settings, as recorded in above.

  • If an auxiliary power supply is being used for the MicroLogic trip unit, reconnect the auxiliary power supply.

Additional Information

For more information concerning Square D Circuit breakers, refer to the appropriate instruction manual. These manuals contain installation instructions, mounting information, safety features, wiring diagrams, and troubleshooting charts for specific circuit breakers.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?