List of IFM Interface Commands

List of Commands

The following table lists the IFM interface commands, their corresponding command codes and user profiles. Follow the command execution procedures accordingly.

Command

Command code

User profile

Get current time

768

No password required

Set absolute time

769

No password required

Read IMU name and location

1024

No password required

Write IMU name and location

1032

Administrator

Set validity duration of data

41868

Administrator, Services, Engineer, or Operator

Error Codes

Error codes generated by the IFM interface are the generic error codes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?