Energy Management using Smart Equipment
Schneider Electric’s exclusive Smart Equipment can be fully directed to company IT networks to help improve energy performance.
This user guide provides basic information on the Enerlin’X system and how it can be used to design, build, and configure Smart Equipment.
The guide can help determine how to equip circuit breakers and other protective devices in the PowerPacT and MasterPacT ranges, depending on the information required from each of them. This guide is a supplement to the other Smart Equipment design and construction documents.
For additional information about Enerlin’X, see catalog 0614CT1802, Enerlin’X Digital Solutions for Smart Systems Catalog.
For additional information about ULP, see user guide DOCA0093EN, ULP (Universal Logic Plug) System User Guide.
For additional information about Modbus, see user guide 0611IB1302, PowerPacT H-, J-, and L-Frame Circuit Breakers — Modbus Communication Guide.
Five Types of Information
Below are definitions of the five types of information available through the Enerlin'X system. First, select the relevant information types for your application, then consult the Data Acquisition section of this document for the equipment options.
Two Ways to Access Information
Communication Accessory Abbreviations
-
BCM: Breaker Communication Module
-
BSCM: Breaker Status and Control Module
-
FDM: Front Display Module
-
IFE: Interface Ethernet Module
-
IFM: Interface Modbus SL Module
-
I/O: Input/Output Module