Scope

 

Single current sensor ground fault systems like (but not restricted to) source ground return (see Figure 1) and VigiPacT™ residual current protection relays (see Figure 2).


Figure 1: Source Ground Return for MasterPacT™


Figure 2: VigiPacT Residual Current Protection Relay




Purpose:

To verify the functionality of a single current sensor ground fault system. The focus is to make sure the system is working, not to pass/fail the system on pickup accuracy, delay accuracy, or metering accuracy as there are too many variables with the power supply, test setup, etc.

Recommendation:

A simple and advance test method is provided below. The simple method is recommended for basic system functionality.

Example Power Supplies:
  • Phoenix

  • MultiAmp

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.