80210–100–12

NEMA 2 Rated Cover Kits Inspection

Inspect the parts for gasket placement (Figure 1). Examples of damaged gaskets are shown in Figure 2.

NOTE: Retain all hardware for reuse.

DANGER
HAZARD OF ELECTRIC Shock or ARC Flash
Damage in gasket can result in arc fault. Replace damaged gasket.
Failure to follow these instructions will result in death or serious injury.

Covers with Gasket

Example of Damaged Gaskets

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?