Protection of Motor Branch-Circuits

To protect the motor branch-circuit against short-circuits, overload relay protection must be coordinated with protection provided by the short-circuit protective device (SCPD). The SCPD may be a fused switch or a circuit breaker. The figure Typical Coordination Curves shows the critical point (Ic) in this coordination.

Operation of the Melting Alloy Overload Relay

As heat melts the alloy, a ratchet wheel is free to turn. The spring then pushes the contacts open.

Typical Coordination Curves

At current values greater than Ic, the SCPD reacts quicker than the overload relay. At current values less than Ic, the overload relay reacts quicker. Refer to Articles 110 and 430 of the NEC for guidance in selecting the SCPD. These articles help with coordinating the components of a motor branch-circuit (such as determining the location of point Ic).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?