ArcFM Markup Pane Markup Information

Publishes in Mobile config, Mobile Tools, Desktop using, EXI

Publishes in all
To display the markup pane, click the Markups button. Be aware that only active markups are displayed. Each markup record displays its current status, who submitted the markup, the date it was submitted, and a number of operational choices. From the markup pane, you can filter markups based on your assigned work, all available work, markup type, and markup name. You can also assign, unassign, or complete markup. For viewing specific markups on the map, there is functionality that allows you to zoom to a particular markup and show just that markup in the map.

Desktop Using and Mobile config and Mobile Tools
TIP: If your markup feature service is ArcGIS for Portal-federated, refer to Esri ’s Use ArcGIS Desktop with Your Portal topic to help you ensure that ArcMap is connected to the correct feature service.

EXI Using Guide only
TIP: If your markup Operational Map is Portal-federated, refer to Esri ’s Use ArcGIS Desktop with Your Portal topic to help you ensure that ArcGIS Pro is connected to the correct Operational Map.

Desktop Using and Mobile config and Mobile Tools

EXI only

Desktop Using and Mobile config and Mobile Tools
IMPORTANT: If your markup map service operates over HTTPS, you may need to install the correct certificate on all Mobile client machines for markups to function properly.

EXI only
When more than 50 markups are available, the Markups pane automatically displays only the first 50 records on both the My Work and Available Work tabs. Click the Load More button at the bottom of the pane to view the next 50 markups. This appends the next 50 markups at the end of the current list. This format allows for a quicker load time when numerous markups are available.
TIP: Search filters on all markups (not just on the current page), however, the search results are not displayed in the same 50 item limit. If you perform a search with more than 50 results, all results are displayed on one page and it may take a few moments for the page to complete loading.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?