Web Configuration for SCADA (optional module)

The table below shows web.config settings used for optional integration with MultiSpeak.

Config Key

Config Description

Config Value

Scada.EventMap

Mapping of SCADA Events defined in MultiSpeak and required in Responder

Scada.EventMap

Scada.RequireDayLightAdjustment

Set this flag if adjustment is required due to Daylight Saving Time.

TRUE

Scada.DayLightOffsetMins

Configure the time adjustment required when Daylight Savings Time is in effect.

60

StaleEventThreshold

EVENTTIME timestamp in HTTP endpoint data received over this threshold compared to system time are not processed and are errored out back to the source system.

02:00:00

MomentaryEventThreshold

Time between Open and Close events that are within this threshold are considered momentary.

00:01:00

ScadaIncidentRemarks

Remarks on incidents created by SCADA.

Created by SCADA.

FilterDuplicates

Multiple incidents will not be created when SCADA events are created for the same device.

TRUE

ScadaClassModelName

Class model name to be assigned to identify the SCADA device in the geodatabase.

SCADAFEATURECLASS

ScadaFieldModelName

Field model name to identify the SCADA Device using the Field assigned this model name.

SCADADEVICEID

IsRegistrationRequired

Configuration flag to determine if the headend AMI system needs an OMS system to request a subscription to receive meter event notifications.

FALSE

AlwaysUnsubscribeAndThenSubscribe

Configuration flag to determine if the AMI headend system is expecting the OMS System to unsubscribe the existing subscription before requesting a new subscription or subscribe regardless of the previous one.

FALSE

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?