Create Engine Login

In this step, you'll use the ArcFM Engine Administrator to create a login to the backdrop database. Perform this step on the Administrator machine. In the next step (Deployment), you'll copy the files necessary to make this login, the replication configuration and all databases available to every field machine.

To create a login to the backdrop database (or login database if you've created one) using the ArcFM Engine Administrator, follow the steps in the topic Login.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?