TransitionPoint
-
ObjectID fields are automatically created (by Esri) when you create the schema.
-
GlobalID fields are required by Fiber Manager and are created with Esri's Add Global ID tool (Manage > Add Global IDs).
-
GlobalID fields must also have the GLOBALID field model name assigned.
-
Enabled fields are automatically added/configured by the geometric network.
-
In ArcGIS applications, there are four numeric data types: Short Integer, Long Integer, Float, and Double. The choices reflect a balance between minimizing storage space while still allowing enough range and precision for the field to be useful. For example, because lengths typically have decimals, these fields are assigned either Float or Double.
In the table below, any field set to integer does need to be either a Short or Long Integer, as these fields cannot contain decimals. So, the decision comes down to the minimum and maximum values you need for the field:
-
Short Integer Storable Range: -32,768 to 32,767
-
Long Integer Storable Range: -2,147,483,648 to 2,147,483,647
So, as an example, would you ever have more than 32,767 patch panels on a single rack? No. So, the RackPosition field for Patch Panels could be a Short Integer. Conversely, foot or meter stamps along a cable could exceed 32,767. So, CableMarking fields for fiber optic cables should be a Long Integer. Our integer recommendations err on the side of more range and usefulness, but your company could decide to change a Long Integer to a Short Integer (or a Double down to a Float) if you knew the maximum values would never exceed the types’ upper threshold.
-
Alias: Transition Point
Type of features: ArcFM Simple Junction Feature
Geometric Network: Ultimately belongs to the Fiber_Network when you Create the Geometric Network later in these steps.
Field |
Data Type |
Default Value |
Domain |
Length/Precision |
---|---|---|---|---|
FiberChildClassModelName Alias: Fiber Child Class Model Name |
Text |
50 |
||
FiberParent Alias: Fiber Parent |
Guid |
|||
FiberParentClassModelName Alias: Fiber Parent Class Model Name |
Text |
50 |
||
RiserFootage Alias: Riser Footage |
Long Integer The data type needs to match the data type of the Fiber Riser Height domain, which is Long Integer in the sample data. If your domain is Short Integer, then use Short Integer instead. |
Fiber Riser Height |
||
SymbolRotation Alias: Symbol Rotation |
Double |
0 |
||
ThisFiberClassModelName Alias: This Fiber Class Model Name |
Text |
TransitionPoint The default value on this field (and only on this particular feature) must be assigned at the subtype level.
|
50 |
Field Display
Primary Display Field: Choose this field in the ArcFM Properties Manager. The chosen field is displayed when using ArcFM tools such as the ArcFM Locator and ArcFM Attribute Editor. Your company can choose the most useful field to display for the end users. If the chosen field is null for the selected or identified features, the display field defaults to the ObjectID.
Model Names
FIBEROBJECT, TRANSITIONPOINT
Field Model Names
FiberChildClassModelName: FIBERCHILDCLASSMODELNAME
FiberParent: FIBERPARENT
FiberParentClassModelName: FIBERPARENTCLASSMODELNAME
GlobalID: GLOBALID
RiserFootage: POINTLENGTH
SymbolRotation: SYMBOLROTATION
ThisFiberClassModelName: THISFIBERCLASSMODELNAME
Object AutoUpdaters
On Feature Create: ArcFM Fiber Optic Cable Splitter; ArcFM Fiber Optic Cable Length; ArcFM Validate Transition Point Creation
On Feature Update: ArcFM Fiber Optic Cable Length
On Feature Delete: ArcFM Fiber Object Deleted
Field Autoupdaters
ChangeDate — On Feature Update: ArcFM Current Date
ChangeUser — On Feature Update: ArcFM Login User Name
CreationDate — On Feature Create: ArcFM Current Date
CreationUser — On Feature Create: ArcFM Login User Name
SymbolRotation — On Feature Create: ArcFM Auto Angle Setter