Electric Field Model Names
|
Model Name |
Object |
|---|---|
|
ACTUALDUCTSIZE |
ActualDuctSize attribute in DuctDefinition object (optional) |
|
AT_<Field Name> |
Any attribute of a source feature class that should be transferred to the abandoned (destination) feature class; must also exist on the corresponding field of the destination feature/object class |
|
BYPASSID |
Assign to duct field of the same name. It tracks connections between ducts when they bypass underground structures. |
|
BYPASSIDFROM |
Assign to the Duct Definition field of the same name. It tracks connections between ducts when they bypass underground structures. |
|
BYPASSIDTO |
Assign to the Duct Definition field of the same name. It tracks connections between ducts when they bypass underground structures. |
|
CLASS |
Assign to attribute that represents class of structure; used for structural analysis |
|
CIRCUITSOURCEGLOBALID |
Assign to the GlobalID field in CircuitSourceID tables. This field and field model name enable Extended Feeder Manager to use Global IDs. |
|
CIRCUITSOURCEGUID |
Assign to the GUID field added to any table except the CircuitSourceID table. This field and field model name enable Extended Feeder Manager to use GUIIDs. IMPORTANT: Do NOT assign this to the CircuitSourceID
table.
|
|
CIRCUITSOURCEID |
Assign to the CircuitSourceID field. This field and field model name are used by Feeder Manager to support multi-tiered networks. |
|
CONDUCTORMATERIAL |
Assign to attribute of ConductorInfo or overhead conductor feature class that represents material of conductor; used for structural analysis |
|
CONDUCTORSIZE |
Assign to attribute of ConductorInfo or overhead conductor feature class that represents size of conductor; used for structural analysis |
|
CONTINUINGDUCTNAME |
Assign to the Duct field of the same name. It tracks connections between ducts when they bypass underground structures. |
|
CONTINUINGDUCTNAMEFROM |
Assign to the Duct Definition field of the same name. It tracks connections between ducts when they bypass underground structures. |
|
CONTINUINGDUCTNAMETO |
Assign to the Duct Definition field of the same name. It tracks connections between ducts when they bypass underground structures. |
|
DEVICETYPE |
Indicates the type of device. Assigned to the DeviceType field on the MMENG_DEVICEWEIGHT field for Structural Analysis (Designer only). |
|
DIAMETER |
The attribute on any overhead support structure feature class that represents the diameter of the structure; used for structural analysis |
|
DUCTAVAILABILITY |
Available attribute in DuctDefinition object |
|
DUCTBANKCONFIGURATION |
DuctBankConfiguration attribute in conduit feature class with ULS model name |
|
DUCTBANKHEIGHT |
Height attribute in DuctDefinition object (optional) |
|
DUCTBANKWIDTH |
Width attribute in DuctDefinition object (optional) |
|
DUCTID |
DuctID attribute in DuctDefinition object (optional) |
|
DUCTMATERIAL |
Material attribute in DuctDefinition object |
|
DUCTNAME |
Name attribute on the Duct feature class |
|
DUCTOCCUPIED |
Occupied field on the Duct feature class |
|
DUCTSIZE |
DuctSize attribute in DuctDefinition object |
|
FACILITYDIAGRAM |
FacilityDiagram field on the UndergroundStructure feature class |
|
FACILITYID |
Assign to FacilityID field of Transformer feature class; used by Secondary Circuit Analysis |
|
FDRMGRGANGOPERATED |
Indicates whether a device is gang operated. |
|
FDRMGRNONTRACEABLE |
The attribute on any feature class that indicates whether a feature should be traced by Feeder Manager. For a detailed explanation of FDRMGRNONTRACEABLE, view the appendix help topic: Appendix > Bitgate Fields > Electric Tracing - Edges. |
|
FEEDERID |
The FeederID field in any network listed as part of a feeder; also the FeederID field in the CircuitSource object |
|
FEEDERID2 |
The FeederID2 field in any network listed as part of a feeder |
|
FEEDERINFO |
The FeederInfo field in any network feature listed as part of a feeder |
|
FEEDERLEVEL |
Assign to the FeederLevel field. This field and field model name are used by Feeder Manager to support multi-tiered networks. |
|
FEEDERNAME |
The FeederName in the CircuitSource object. |
|
FEEDERSOURCEINFO |
The FeederSourceInfo field in the CircuitSource object |
|
GROUNDREACTANCE |
Ground reactance field of Transformer |
|
GR0UNDRESISTANCE |
Ground resistance field of Transformer |
|
GUYCOUNT |
Assign to attribute on AnchorGuy feature class that represents the number of guys in the system; used for structural analysis |
|
HASSUBDUCTS |
HasSubducts field on the Duct feature class |
|
HEIGHT |
Assign to attribute on AnchorGuy feature class that represents the height of the structure; used for structural analysis |
|
HIGHSIDECONFIGURATION |
Assign to HighSideConfiguration field of Transformer |
|
HIGHSIDEGROUNDREACTANCE |
Assign to HighSideGroundReactance field of Transformer |
|
HIGHSIDEGROUNDRESISTANCE |
Assign to HighSideGroundResistance field of Transformer |
|
INSULATIONTYPE |
Assign to insulation type field |
|
JOINTATTACHMENTOWNER |
Assign to the Owner field of the JointUseAttachment table |
|
LASSOTEXT |
The LassoText field in the Lasso feature class (ULS/contents relate tool) |
|
LASSOTEXTFIELD |
Assign to field that is source for a different label than label in the contents list of cross section annotation feature for a conductor or cable feature class contained in a conduit system |
|
LEADLENGTH |
Assign to lead length field |
|
LOWSIDECONFIGURATION |
Assign to LowSideConfiguration field of Transformer |
|
LOWSIDEGROUNDREACTANCE |
Assign to LowSideGroundReactance field of Transformer |
|
LOWSIDEGROUNDRESISTANCE |
Assign to LowSideGroundResistance field of Transformer |
|
LOWSIDEVOLTAGE |
Assign to LowSideVoltage field of Transformer |
|
MANUFACTURERMODEL |
Assign to the Manufacturer Model field in the MMENG_DEVICEWEIGHT table for Structural Analysis. Designer only. |
|
MATERIAL |
Assign to attribute on overhead support structure feature class that represents the material; used for structural analysis |
|
MMELECTRICTRACEWEIGHT |
Assign to electric trace weight field of features participating in Feeder Manager and electric trace tasks |
|
MMSECCKTAMPACITY |
Assign to Ampacity field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTCODE |
Assign to Code field of MMENG_TRANSFORMER and MMENG_CONDUCTOR_ELEC tables; used for secondary circuit analysis |
|
MMSECCKTCOST |
Assign to Cost field of MMENG_TRANSFORMER and MMENG_CONDUCTOR_ELEC tables; used for secondary circuit analysis |
|
MMSECCKTCUCODE |
Assign to CUCode field of MMENG_TRANSFORMER and MMENG_CONDUCTOR_ELEC tables; used for secondary circuit analysis |
|
MMSECCKTDESCRIPTION |
Assign to Description field of MMENG_TRANSFORMER and MMENG_CONDUCTOR_ELEC tables; used for secondary circuit analysis |
|
MMSECCKTINSULATION |
Assign to Insulation field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTMATERIAL |
Assign to Material field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTR_PER1000UNITSLENGTH |
Assign to R_Per1000_Units_Length field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTR0_PER1000UNITSLENGTH |
Assign to R0_Per1000_Units_Length field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTSIZE |
Assign to CondSize field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERFULLLOADLOSSMAX |
Assign to FULL_LOAD_LOSS_MAX field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERNOLOADLOSSMIN |
Assign to FULL_LOAD_LOSS_MIN field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERKVA |
Assign to kVA field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERMAXXTOR |
Assign to X_TO_R_MAX field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERMAXZ |
Assign to Percent_Z_MAX field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERMINXTOR |
Assign to X_TO_R_MIN field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERMINZ |
Assign to Percent_Z_MIN field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERNOLOADLOSSMAX |
Assign to NOLOAD_LOSS_MAX field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERNOLOADLOSSMIN |
Assign to NOLOAD_LOSS_MIN field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTTRANSFORMERPHASES |
Assign to Phasing field of MMENG_TRANSFORMER table; used for secondary circuit analysis |
|
MMSECCKTUNDERGROUND |
Assign to Underground field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTX_PER1000UNITSLENGTH |
Assign to X_Per1000_Units_Length field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
MMSECCKTX0_PER1000UNITSLENGTH |
Assign to X0_Per1000_Units_Length field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis |
|
NEUTRALMATERIAL |
Assign to attribute on overhead support structure feature class that represents the material of neutral cable; used for structural analysis |
|
NEUTRALSIZE |
Assign to attribute on overhead support structure feature class that represents the size of the neutral cable; used for structural analysis |
|
NOMINALVOLTAGE |
Used by the ArcFM Inherit Nominal Voltage autoupdater. Assign to the Nominal Voltage field on the Primary Conductor and Transformer feature classes. |
|
NORMALPOSITION_A |
The attribute on all switchable feature classes (e.g., fuse, switch) that indicates the position (open or closed) of phase A |
|
NORMALPOSITION_B |
The attribute on all switchable feature classes (e.g., fuse, switch) that indicates the position (open or closed) of phase B |
|
NORMALPOSITION_C |
The attribute on all switchable feature classes (e.g., fuse, switch) that indicates the position (open or closed) of phase C |
|
NUMBERCONDUCTORSPERPHASE |
Assign to attribute on ConductorInfo or overhead conductor feature class that represents the number of conductors present for each phase; used for structural analysis |
|
OPERATINGVOLTAGE |
The attribute on any conductor feature class or bus bar feature class that indicates the operating voltage of the feature |
|
PARENTCIRCUITSOURCEGUID |
Assign to the GUID field added to any table, including any CircuitSourceID table, that had the field model name PARENTCIRCUITSOURCEID assigned to a field. Used by Extended Feeder Manager to support the use of GlobalIDs. |
|
PARENTCIRCUITSOURCEID |
Assign to the ParentCircuitSourceID field. This field and field model name are used by Feeder Manager to support multi-tiered networks. |
|
PHASEDESIGNATION |
The attribute on any Conduit System member that indicates the phase of the feature (to support Conduit System Management); the attribute on any transformer feature class or load point feature class (e.g., PrimaryMeter) that indicates the phase of the feature (to support Feeder Manager); the attribute on any conductor that indicates the phase of the conductor (to support the Auto Phase Assign autoupdater) |
|
RATEDKVA |
The RatedKVA field in the DistributionTransformer feature class and the TransformerUnit object |
|
RATING |
Assign to the Rating field in the MMENG_DEVICEWEIGHT table for Structural Analysis. Designer only. |
|
RELATEDFEATURECLASSNAME |
Assign to the RelatedFeatureClassName field. This field and field model name are used by Feeder Manager to support multi-tiered networks. |
|
RELATEDOBJECTID |
Assign to the RelatedObjectID field. This field and field model name are used by Feeder Manager to support multi-tiered networks. |
|
SERIALNUMBER |
Assign to the Serial Number field in the MMENG_DEVICEWEIGHT table for Structural Analysis. Designer only. |
|
SERVICECURRENTRATING |
Assign to service current rating field; used by secondary circuit analysis |
|
STRUCTUREFLOORLENGTH |
Assign to Underground Structure field of the same name. This allows the Create Floors and Walls tool to consume dimensions from the attributes of the structure, instead of needing to by personally typed by the end user. |
|
STRUCTUREFLOORWIDTH |
Assign to Underground Structure field of the same name. This allows the Create Floors and Walls tool to consume dimensions from the attributes of the structure, instead of needing to by personally typed by the end user. |
|
STRUCTUREWALLHEIGHT |
Assign to Underground Structure field of the same name. This allows the Create Floors and Walls tool to consume dimensions from the attributes of the structure, instead of needing to by personally typed by the end user. |
|
SUBSOURCE |
Assign to the SubSource field. This field and field model name are used by Feeder Manager to support multi-tiered networks. |
|
SUBSTATIONID |
The SubstationID field in the CircuitSource object |
|
SUBTYPECD |
The field on the Duct Definition object class that indicates the subtypes defined |
|
SYNCDUCTCUSTOMFIELDSBYNAME |
Assign to the Duct Definition field of the same name. This tracks custom fields between the Duct Definition table and the Duct feature class the various Conduit Manager dialogs. |
|
ULSTEXTFIELD |
In a ULSMember, designates field used for display in Cross Section contents list (optional) |
|
USAGETYPE |
The attribute on any overhead support structure feature class that represents the type of use of the structure; used for structural analysis |
|
WALLGRIDORIGIN |
Assign to the Wall feature class field of the same name. This lets the Wall Editor > Grid Configuration be saved by wall, which allows walls to have different grid arrangements that persist. |
|
WALLGRIDCELLSIZE |
Assign to the Wall feature class field of the same name. This lets the Wall Editor > Grid Configuration be saved by wall, which allows walls to have different grid arrangements that persist. |
|
WIRESIZE |
Assign to attribute on AnchorGuy that represents the guy wire size; used for structural analysis |
|
WIRESTRENGTH |
Assign to attribute on AnchorGuy that represents the guy wire strength classification; used for structural analysis |