Edit Highlight Properties

Publishes in Mobile config

Follow the steps below to edit the properties for a layer that has a transparency value:

  1. Open the Properties dialog for the layer.
  2. Click the Display tab.
  3. Type the desired transparency in the Transparent field.
  4. Click OK.

Once you're satisfied with the configuration for markups, save it to an MXD file or to a Stored Display to make the viewing of future ArcMap markup sessions more convenient. If you save to an MXD, and you want other users to have access to it, save it to a shared location.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?