Find Incident for Customer

Available in Responder Explorer.

The Find Incident For Customer button allows you to locate a specific customer and determine whether an incident exists for that client.

  1. Click Find Incident For Customer on the Responder Toolbar in Responder Explorer.

    The User Inputs dialog appears.

  2. Provide search criteria.
  3. Click OK.

    Found records appear in a separate window. This list includes all customer records that fit the criteria, whether incidents exist or not.

  4. Double-click the customer row to open the corresponding incident in Responder Explorer (if an incident exists for that customer).
    NOTE: If the customer resides at a multi-customer loadpoint (e.g., apartment building), the incident is identified in the search, regardless of whether that specific customer has been selected as out.

    If no incidents exist for the customer, the following message appears in the lower-left corner of the Select a Customer window:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?