RX_INCIDENT_CAUSE_STATISTICS_ARCHIVE
Field Name |
Description |
CAUSE |
Indicates the cause of the outage. This field uses the CAUSE domain. |
CAUSE_DESCRIPTION |
A description of the type of event that caused the incident. |
SAIDI |
Stands for System Average Interruption Duration Index, this field reports the average length of time customers were without power for the incident. |
DURATION_SUM |
The sum of durations all customers were without power. |
CUSTOMER_SERVED |
Total number of customers served. |
OUTAGE_COUNT |
Number of distinct customer outages. |