RX_PREVIOUS_INCIDENTS_ARCHIVE
Field Name |
Description |
TIME_OUTAGE |
The time the outage occurred. |
TIME_RESTORED |
The time the customer's power was restored. |
DURATION |
Indicates the weather at the incident site. This field uses the WEATHER domain. |
CHANGE_DATE |
The time and date an operation was performed on the record. |
HAZARD |
Indicates any hazards in the area (e.g., fire, wires down, etc.). This field uses the HAZARD domain. |
CAUSE |
Indicates the cause of the outage. This field uses the CAUSE domain. |
WEATHER |
Indicates the weather at the incident site. This field uses the WEATHER domain. |
INCIDENT_ID |
The ID associated with the incident. This field corresponds with the ID field in the RX_INCIDENTS table. |
REMARKS_DISPATCH |
Remarks from the dispatcher. |
REMARKS_FIELD |
Remarks from the field crew. |