Available Tasks Tool
Available in: ArcFM (Process Tasks toolbar), ArcFM Viewer for ArcGIS Engine, Session Manager, Workflow Manager
Enable: Open a session or design in ArcFM or ArcFM Viewer. In Session Manager and Workflow Manager, this tool is always enabled.
The Task tool offers an easy method for performing actions in your
Process Framework extension. When you select a node, the Available
Tasks tool dropdown menu shows the actions that may be performed on
that node. Simply select a node, choose a task from the menu, and
click the Execute Task button.
The figure below shows Available tasks in Session Manager.

The following figure shows ArcFM Process Tasks toolbar in ArcFM

The ArcFM Process Tasks toolbar (is not available in ArcFM Viewer for ArcGIS Engine. The Available Tasks tool appears on the Session Manager toolbar instead (shown below).
The figure below shows the Available tasks on the Session Manager toolbar in ArcFM Viewer for ArcGIS Engine

The current install includes sample subtasks for Session Manager and Workflow Manager. Your administrator may also create and edit Tasks using the Process Framework Administration tool (see the online help for the Admin tool). Descriptions of the sample subtasks provided are available in the Set Up Process Framework Tools section of the Configuring ArcFM Solution online help in ArcCatalog.