Primary Functions

EcoStruxure™ Asset Performance Management offers an intuitive user interface and these functions.

Asset Models
Asset descriptive data including asset category, asset class, and location data.
Network Model
Asset location hierarchy and map view.
Condition Assessment
Algorithms and rules to calculate health index based on observed, measured, and computed field data (e.g., Dissolved Gas Analysis (DGA) of oil insulated transformers).
Asset Aging
Methodology to evaluate the apparent asset age considering the condition in which it operates.
Health Index
Calculation of asset health index leveraging the UK Distribution Network Operators (DNO) Office of Gas and Electricity Markets (OFGEM) Common Asset Indices Methodology standard, taking into consideration:
  • Location factor (distance from coast, altitude, indoor/outdoor installation)

  • Duty factor (asset utilization rate vs. nominal ratings)

  • Health modifiers (age, observed conditions, measured conditions)

  • Reliability modifier (Utility specific rule)

Probability of Failure
Calculation of asset likelihood to fail using one or a combination of: condition assessment, predictive model, aging, CNAIM.
Consequence of Failure
Asset criticality assessment defined in the UK DNO OFGEM Common Asset Indices Methodology standard, and taking into account:
  • Financial consequences (costs to have the asset repaired and back to operations after failure)

  • Safety consequences (costs of injury/death of staff/public caused by asset failure)

  • Environmental consequences (costs of oil leakage, SP6 leakage, fire hazard or produced waste caused by asset failure)

  • Network performance consequences (costs of non-delivered energy)

Risk Assessment
Delivery of risk matrix combining asset probability of failure with criticality/consequences. Matrix shows the quantity of assets plotted in the matrix and supports maintenance/repair/replace decisions.
Investment scenarios
Generation of a multi-year investment scenario considering the asset performance, risk analysis and additional criteria such as budget and resources availability.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.